Results for ‘k33’
-
FLIR K33 Support
Enhanced 2024 Model FLIR now gives you a low-cost, easy-to-use option that doesn't sacrifice the reliable clarity and performance you need - the FLIR K33. This TIC features FSX Flexible Scene Enhancement, which intensifies structural and textural details in thermal images. The enhanced perspective and orientation helps improve situational awareness and give firefighters a greater sense of confidence and safety.
-
2-5-10 Warranty for FLIR K33, K45, K53, K55, K65, K2 Thermal Cameras
FLIR K33, K45, K53, K55, K65, and K2 handheld firefighting thermal imaging cameras are covered by our revolutionary 2-5-10 Warranty when registered within 60 days of purchase.
-
Is it possible to change the object parameters in K series cameras?
Object parameters in the FLIR K series are set to the following and are not possible to change.
-
What are the environmental specification for Flir K series?
-
What is the temperature measurement accuracy for the Flir K series?
The specified accuracy is ±4°C (±7.2°F) or ±4% of reading, for ambient temperature +10°C to +35°C (+50°F to +95°F).
-
Working with Estonian Fire Service for 10 Years
For 10 years Teledyne FLIR has established excellence in the field of fire fighting by tailoring our K-series cameras to those who run in first. From image quality to ease-of-use and intense durability, our cameras have satisfied first responders throughout the years to make their job easier and ensure safety. Learn about the difference FLIR has made with the Estonian Fire Service from our video below.
-
Thermal Imaging for Hydrogen Flame Detection and Monitoring
Renewable hydrogen is set to play a crucial role in the energy transition. European member states are already experimenting with this promising energy carrier, and they are testing how they can repurpose existing natural gas distribution networks to bring hydrogen to the consumer. Hydrogen is a highly flammable gas. That is why technical staff working on these hydrogen distribution networks will need to be trained for safety. They will also need to be equipped with the right tools to detect hydrogen leaks and see hydrogen flames in time. One such tool is the thermal imaging camera.
-
Are the batteries in FLIR cameras allowed on board airplanes?
If you are traveling with your IR camera or other battery-operated equipment to, from or within the USA - and perhaps elsewhere around the world - the U.S. Department of Transportation's (DOT) recent pronouncements about the rules governing the transport of batteries containing Lithium means you may have to plan a bit more carefully how many rechargeable battery packs you carry with you, and how you carry them.
-
K-Series Software
-
Teledyne FLIR cameras help save lives in Stockholm fire
Firefighting is an extremely dangerous and demanding profession, both physically and mentally. The team at Solna Fire Station in Stockholm, Sweden, is a case in point, where the use of a FLIR K-series camera recently helped one of the team’s smoke divers save four lives in a city centre fire.
-
Download FLIR K-Series Software & Firmware
-
What is the highest object temperature the FLIR K series can see?
The second temperature range goes up to 650°C/1202°F. When the object temperature is above 650/1202°F°C the text >650°C or >1202°F will be displayed on the screen and any temperatures above 650°C/1202°F will have a dark red color.