What is the highest object temperature the FLIR K series can see?
The second temperature range goes up to 650°C/1202°F. When the object temperature is above 650/1202°F°C the text >650°C or>1202°F will be displayed on the screen and any temperatures above 650°C/1202°F will have a dark red color. See the picture below.
Related Articles
Application Story
Lawrence, Massachusetts Deploys FLIR Video System for Safety