![](/globalassets/industrial/oem/adk/answers/415qd040.bmp) |
The heat detection mode is optimized for searching hotspots during overhaul after the fire is out—typically to ensure that there is no hidden fire left. This mode can also be used to find thermal patterns, for example signs of people in car seats after accidents, to ensure that everyone has been found. This mode can also be used to search for people in water and open landscapes.
- High-sensitivity range only.
- Colorization of heat: the 20% highest temperatures in the scene.
- High-sensitivity range: –20 to +150°C (–4 to +302°F).
|