Using the Silent Installer for the Spinnaker SDK

The Spinnaker SDK is a comprehensive development kit designed to empower developers in creating cutting edge and reliable vision solution. Recognizing the importance of efficient deployment, the SDK includes a silent installer, a specialized tool that significantly simplifies the installation process, especially in complex environments with multiple systems or automated workflows.

Spinnaker4-silent-installerv3.gif

Why Silent Installation Matters

Silent installers are specifically engineered to operate without requiring any user interaction or graphical interface prompts. This "hands-off" approach brings a range of benefits to the deployment of the Spinnaker SDK:

  • Optimized Deployment: In scenarios where the SDK needs to be installed on a large number of machines or integrated into automated setup processes, silent installation dramatically reduces the time and effort required. It eliminates the need for manual input on each target machine, resulting in faster and more efficient deployment.
  • Error Mitigation: Human error is a common risk during manual installations. With silent installers, the possibility of incorrect inputs, skipped steps, or other user-induced issues is virtually eliminated. This leads to a more reliable and consistent deployment experience.
  • Tailored Installations: Silent installers offer flexibility through configuration options. Developers can customize the installation process by specifying parameters such as the installation directory, the selection of specific components, and other relevant settings. This allows for tailored installations that meet the unique requirements of different systems or use cases.

Technical Details

The silent installer included in the Spinnaker SDK adheres to industry best practices and utilizes command-line parameters to control the installation procedure.

Command-Line Parameters (Examples)

  • /install /silent: Activates silent installation mode.
  • /uninstall /silent: Activates silent uninstaller mode

Example Usage

Command line:
SpinnakerSDK_FULL_4.0.0.116_x64.exe /install /silent Features=Runtimes_v140,GigEDrivers

For more installation options, please refer to Distributing Spinnaker Applications.

Important Considerations

  • Administrative Rights: Silent installations typically necessitate elevated privileges (administrator rights) to execute successfully.
  • Dependencies: Before initiating the silent installation, ensure that any prerequisite software is already present on the target machine.
  • Log Analysis: The installation log file, default directory C:\ProgramData\Spinnaker\Logs, serves as a valuable resource for diagnosing and troubleshooting any issues that may arise during the process.

Conclusion

The silent installer is an indispensable component of the Spinnaker SDK, contributing significantly to the ease and efficiency of the deployment process. By automating and refining installation procedures, it enables developers and administrators to achieve greater productivity, reliability, and scalability in the development and deployment of machine vision applications.

By incorporating the silent installer into your deployment strategy, you unlock a powerful tool that enhances the overall efficiency and effectiveness of your project.

Related Articles