Teledyne FLIR IIS Dragonfly S camera now in full production
The Dragonfly®️ S provides solutions for industries ranging from factory automation to medical imaging.
![](/globalassets/industrial/iis/machine-vision/dragonfly-s/press-release/product-press-release-images-2.png)
Richmond, CANADA – August 7, 2024 – Teledyne FLIR IIS, a Teledyne Technologies [NYSE:TDY] company, is pleased to announce that its Dragonfly®️ S USB 5MP modular and compact camera is now in full production.
The Dragonfly S 5MP is the first camera in the new Dragonfly S series to enter full production. Designed as an entry point for machine vision applications, the Dragonfly S streamlines rapid prototyping of imaging systems and ensures smooth transition into production manufacturing. The cameras are optimized for size, weight, power, and cost, addressing fundamental machine vision application needs without unnecessary complexity. The cameras are ideal for a range of applications from industrial automation and robotics to medical imaging and scientific research.
The new Dragonfly S camera series is cost-optimized while maintaining high quality and reliability. The cameras are supported by the Spinnaker® 4 SDK and are GenICam compliant. The on-board buffer ensures reliable data transmission to the host system, preventing incomplete or dropped images. In environments with low EMI tolerance, such as laboratories or hospitals, the full-case cameras are EMC Class B compliant and eliminate the need for additional EMI shielding. For embedded applications, the cameras can extend USB3 bus power to drive peripherals like small LEDs and electronics (up to 120mA) via the GPIO port with minimal cabling.
A complete evaluation kit is available for CS-mount camera variants to facilitate camera selection, enabling the creation of seven distinct camera configurations. The kit includes adapters for C and S mount optics, along with components for assembling full-case, partial- case or board level variants.
For more information about the Dragonfly S models visit the Discover Page
See live demonstrations of Dragonfly S cameras at these upcoming events:
- Automation Expo 2024, August 21-24, 2024 | Hall 2 N1, N2 | Bombay Exhibition Center | Mumbai, India
- VISION, October 8-10, 2024 | Booth 8B10 | Messe Stuttgart | Stuttgart, Germany
About Teledyne FLIR IIS
Teledyne FLIR IIS (Integrated Imaging Solutions), a Teledyne Technologies company, designs, develops, manufactures, markets, and distributes industrial-grade technologies that enhance productivity and development. The company provides innovative sensing solutions through machine vision, spherical imaging, and stereo-imaging technologies. Teledyne FLIR IIS offers a diversified portfolio that serves a wide variety of applications in industrial, medical, geospatial, and advanced robotics markets. For more information, visit the homepage.
Media Contact:
Farhad Kazi