Teledyne FLIR IIS commits to offering best-in-class imaging solutions for demanding factory automation applications
Next generation camera platform and imaging software leverage years of machine vision GigE camera design expertise and customer understanding to deliver best-in-class imaging reliability, quality, and performance.
![](/globalassets/industrial/iis/machine-vision/spinnaker-sdk/spinnaker/2024-01-02_tdy-flir_spinnaker-software-screen-on-laptop.png)
Richmond, CANADA – January 5, 2024 – Teledyne FLIR IIS is committed to revolutionizing machine vision in factory automation applications. Advancements in industrial automation require machine vision technologies to work in extreme environments while ensuring the production capabilities are highly efficient. Teledyne FLIR IIS is bringing together Teledyne’s long-standing imaging expertise, deep factory automation knowledge, and a focus on innovation and customer success, to alter the factory automation market landscape and transform how machine vision is used.
“Teledyne FLIR IIS is committed to launching imaging technologies that will build the future of machine vision,” said Sadiq Panjwani, General Manager at Teledyne FLIR IIS. “We stay focused on enhancing customer experience to deliver best-in-class imaging reliability and performance – for both our industrial and non-industrial customers.”
The latest Teledyne FLIR IIS imaging product releases are architected to work under extreme conditions ensuring constant reliability without compromising imaging performance
Spinnaker™. Spinnaker 4 is the next-generation GeniCam3 API library for machine vision developers to evaluate, test, and deploy products quickly with the highest performance and reliability. The new software release includes groundbreaking advancements in GigE camera performance and reliability, leveraging Teledyne’s decades of experience delivering best-in-class machine vision GigE cameras worldwide. Intense camera system performance testing, including operating imaging systems with 40 GigE cameras continuously for multiple days at a time, resulted in no incomplete images. Flawless image capture is maintained even when pushing the system CPU usage to over 90%, with intensive image processing and multiple background applications. The software enables fast camera detection and image processing, and much more. For more information, visit our website.
Forge™. Teledyne FLIR IIS’s newest camera platform, Forge, utilizes Spinnaker’s new software architecture and is available in a variety of camera models across multiple sensors. Forge is designed to easily build robust and powerful imaging systems – faster. It offers flexible link speeds as well as the ability to go beyond 5GigE performance and control data transfer to the host. For more information, visit our website.
These latest imaging innovations from Teledyne FLIR IIS represent the start of real change in the factory automation market with new options for best-in-class imaging reliability, quality, and performance.
About Teledyne FLIR IIS
Teledyne FLIR IIS (Integrated Imaging Solutions), a Teledyne Technologies company, designs, develops, manufactures, markets, and distributes industrial-grade technologies that enhance productivity and development. The company provides innovative sensing solutions through machine vision, spherical imaging, and stereo-imaging technologies. Teledyne FLIR IIS offers a diversified portfolio that serves a wide variety of applications in industrial, medical, geospatial, and advanced robotics markets. For more information, visit www.teledyneflir.com/mv.
Media Contact
Farhad Kazi, Marketing Communications Specialist
farhad.kazi@teledyne.com