Teledyne FLIR Object Detection and Tracking Software Accelerates Thermal Camera Integration for ADAS and Autonomous Vehicles
![](/contentassets/eaca60b19bc94a56bf816c4465c9df78/prismai_articleimage_v2.jpg)
Prism™ AI software for automotive thermal perception system development allows for faster integration, testing, and time-to-market
GOLETA, Calif. and New Orleans, LA., June 21, 2022 ― Teledyne FLIR, part of Teledyne Technologies Incorporated, today announced the release of Prism AI, a software framework that provides classification, object detection, and object tracking, enabling perception engineers to quickly start integrating thermal cameras for advanced driver assistance systems (ADAS) and autonomous vehicle (AV) systems. Built for automotive perception system developers, Prism includes features such as visible-and-thermal image fusion and advanced thermal image processing capabilities that provide superior pedestrian and animal detection in challenging lighting conditions. This feature is especially effective at night, which is when more than 79 percent of pedestrian deaths occurred in 2020.
“The Prism AI software model has performed successfully in third-party, NCAP automatic emergency braking (AEB) tests and will now help perception engineers create more effective systems,” said Michael Walters, vice president product management, Teledyne FLIR. “Combining the Prism AI development tools, plugins, and dataset development offers integrators a route to quickly test and decrease development cost for thermal-enabled ADAS or AV that will help save lives.”
Developers can use Prism AI as the primary perception software or as reference software during in-house development. A suite of Prism AI tools provides simplified data integration with the recently released Teledyne FLIR Conservator™ data lifecycle management software as well as the industry’s largest thermal-and-visible training dataset. Compatible with Teledyne FLIR market-leading thermal cameras including Boson®, Tau® 2, and the FLIR ADK™, Prism AI also includes production-required features including authentication between the thermal camera and the electronic control unit, further simplifying development.
By providing the basis for efficient perception model development, Prism AI can also help lower compute cost for commonly used desktop and embedded processors from NVIDIA, Ambarella, Qualcomm, and more. Paired with the Teledyne FLIR expert technical services team available for integration support, perception engineers from academia to OEMs now have a complete ecosystem to build thermal-enabled ADAS and AV systems.
In the United States, preliminary data from the first half of 2021 from the Governors Highway Safety Association estimated a 17 percent increase in pedestrian fatalities compared to the previous year and a 46 percent jump from 2011. Thermal-enhanced ADAS and AV systems can play a crucial role in driving down the unacceptable number of pedestrian traffic fatalities and will aid automotive OEMs to meet upcoming regulatory testing procedures that include nighttime pedestrian front crash prevention.
The Teledyne FLIR Prism AI software is available for purchase globally from Teledyne FLIR. To learn more visit https://www.flir.com/prism.
For an exclusive in-person first look at the Prism AI, please visit booth #1418 at CVPR, June 21-23, 2022, in New Orleans, Louisiana.
# # # #
About Teledyne FLIR
Teledyne FLIR, a Teledyne Technologies company, is a world leader in intelligent sensing solutions for defense and industrial applications with approximately 4,000 employees worldwide. Founded in 1978, the company creates advanced technologies to help professionals make better, faster decisions that save lives and livelihoods. For more information, please visit www.teledyneflir.com or follow @flir.