Professional Media created with FLIR Infrared Cameras
Looking to use thermal imaging for a commercial, TV show, or music video?
Play the videos from our gallery below to see how our thermal cameras are vastly different than typical video cameras.
Hyundai Sonata Turbo 2015
Filmed with FLIR SC8313 HD Thermal Camera. Watch amazing FLIR HD thermal imagery of the new Hyundia Sonata Turbo as it races through downtown city streets. The imagery is spectacular!
Nike - Therma-Sphere Max Commercial
Filmed with a FLIR SC8313 HD Thermal Camera. Nike uses FLIR’s SC8313 HD thermal camera to film a commercial for the introduction of their Therma-Sphere Max thermoregulating composite technology designed for cold weather training. The blending of visual and thermal during high speed athletic training with Victor Cruz really helps show how well their new Therma-Sphere Max technology works to keep the athlete warm.
Coldplay Music Video - "Midnight"
The song Midnight from Coldplay’s new album Ghost Stories was filmed almost entirely in HD thermal using FLIR’s SC8303 thermal camera. Though being in grayscale it might appear as a standard visual camera, it is mostly all thermal footage. Artistically, they chose grayscale and a blue color palettes for the thermal footage.
Earl Sweatshirt Music Video - "Grief"
Filmed with a FLIR SC8313 HD Thermal Camera. In February of 2015, ApplyIR worked on a music video with Doomsday Productions and director Hiro Murai in Los Angeles. The video for rap artist, Earl Sweatshirt's,"Grief" was shot completely in thermal with a FLIR SC8313 on Steadicam. This video shows the power of HD infrared looking at human subjects, snakes, flames, and clown drum circles! (Warning: Strong Language)
NatGeo Wild – Animal Superpowers: Extreme Hunters
Filmed with a FLIR SC8313 HD Thermal Camera
Fox NASCAR Thermal Cam
Filmed with FLIR SC8313 HD Thermal Camera. Courtesy of our friends at FOX, thermal imagery (thermographic) from Kasey Kahne's pit stop. Hot tires off, cold tires on!
Emily Haines & Soft Skeleton Music Video – "Our Hell"
Filmed entirely in HD thermal using FLIR’s A8303sc camera. They chose a grayscale color palette for the thermal footage, and used high contrast targets such as hot or cold liquids and fire to create some interesting imagery.
NASCAR Sprint Cup 2014 – Daytona 500 Car Crash
Filmed with FLIR SC8313 HD Thermal Camera. Check out NASCAR on FOX's thermal cam coverage of the massive wreck on the final lap of Budweiser Duel 2.