Tau 2 WFOV Lens Focus Tool (421-0037-00)

The Tau Focus Tool can be used to change the focus of the wide field of view (WFOV) 5.5mm, 7.5mm, 9mm, 13mm, or 19mm lenses.

Tau 2 WFOV Lens Locking Ring (421-0041-00)

The Tau WFOV Lens Locking Ring is designed to allow a WFOV Tau camera to be bulkhead-mounted. The outside of the lens holder provides M29 x 1.0 threads. By placing the lens through the clearance hole in a bulkhead, the locking ring attaches to the threads to secure the camera to the bulkhead. A Type 2 -025 O-ring should be used between the bulkhead and the Lens Locking Ring to achieve a weatherized seal. This O-ring is not available from FLIR, but is a standard O-ring sold by many suppliers.

Tau 2 WFOV Lens Locking Ring Tool (421-0042-00)

The Tau WFOV Lens Locking Ring Tool is used to install/remove the Lens Locking Ring. It is designed with four ‘nubs’ or pins that mate to the notches in the Lens Locking Ring, allowing the Ring to be easily rotated.

Tau SDK

Software Development Kit

The FLIR SDK allows customers the capability to integrate software that can communicate and perform camera functions. There are 2 main components that comprise the FLIR SDK: Windows Host SDK and Embedded Host SDKM. The Windows Host SDK provides source code (C, C++), samples(C++, C# VB), and binaries (DLL's) that aid customers in the development of camera integration software in a Microsoft Windows OS environment.The Embedded Host SDK provides low level source code written in C, that allows the developer to integrate the SDK with the FLIR camera on a non-Windows OS. Standard driver interfaces are provided by the SDK source code, but the low level drivers (e,g UART) need to supplied by the developer.

Tau Tripod Mount Adapter (261-2071-00)

This adapter allows you to convert two of the mounting points on the Tau camera to a standard 1/4" x 20 tripod mounting plate.